EmberAfInterpanHeader Struct Reference
Interpan header used for sending and receiving interpan messages.
#include <
af-types.h
>
Interpan header used for sending and receiving interpan messages.
Field Documentation
EmberAfClusterId EmberAfInterpanHeader::clusterId |
Referenced by interpanCommand()
, and interpanLongCommand()
.
EmberMulticastId EmberAfInterpanHeader::groupId |
The groupId is only used for EMBER_AF_INTERPAN_MULTICAST
Referenced by interpanCommand()
.
EmberEUI64 EmberAfInterpanHeader::longAddress |
MAC addressing For outgoing messages this is the destination. For incoming messages it is the source, which always has a long address.
Referenced by interpanLongCommand()
.
EmberAfInterpanMessageType EmberAfInterpanHeader::messageType |
EmberAfInterpanOptions EmberAfInterpanHeader::options |
Referenced by interpanLongCommand()
.
EmberPanId EmberAfInterpanHeader::panId |
Referenced by interpanCommand()
, and interpanLongCommand()
.
EmberAfProfileId EmberAfInterpanHeader::profileId |
APS data
Referenced by interpanCommand()
, and interpanLongCommand()
.
EmberNodeId EmberAfInterpanHeader::shortAddress |
Referenced by interpanCommand()
.
The documentation for this struct was generated from the following file:
af-types.h