EmberAfPluginMessagingClientMessage Struct Reference
#include <
af-types.h
>
Data Fields | |
bool | valid |
bool | active |
EmberAfPluginEsiManagementBitmask | esiBitmask |
uint8_t | clientEndpoint |
uint32_t | messageId |
uint8_t | messageControl |
uint32_t | startTime |
uint32_t | endTime |
uint16_t | durationInMinutes |
uint8_t | message [EMBER_AF_PLUGIN_MESSAGING_CLIENT_MESSAGE_SIZE+1] |
Field Documentation
bool EmberAfPluginMessagingClientMessage::active |
uint8_t EmberAfPluginMessagingClientMessage::clientEndpoint |
uint16_t EmberAfPluginMessagingClientMessage::durationInMinutes |
uint32_t EmberAfPluginMessagingClientMessage::endTime |
EmberAfPluginEsiManagementBitmask EmberAfPluginMessagingClientMessage::esiBitmask |
uint8_t EmberAfPluginMessagingClientMessage::message[EMBER_AF_PLUGIN_MESSAGING_CLIENT_MESSAGE_SIZE+1] |
uint8_t EmberAfPluginMessagingClientMessage::messageControl |
uint32_t EmberAfPluginMessagingClientMessage::messageId |
uint32_t EmberAfPluginMessagingClientMessage::startTime |
bool EmberAfPluginMessagingClientMessage::valid |
The documentation for this struct was generated from the following file:
af-types.h