Macros

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_UPDATE_TC_LINK_KEY_PLUGIN_UPDATE_TC_LINK_KEY_TIMER
 plugin update-tc-link-key timer [timeInMilliseconds:4]

Detailed Description

The update trust center link key commands are used to manipulate the behavior of the joining device to attempt the trust center link key updates in a certain fashion.

Macro Definition Documentation

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_UPDATE_TC_LINK_KEY_PLUGIN_UPDATE_TC_LINK_KEY_TIMER

plugin update-tc-link-key timer [timeInMilliseconds:4]

  • This sets the the amount of time between subsequent trust center link key updates in milliseconds.
    • timeInMilliseconds - INT32U - The amount of time between subsequent trust center link key updates in milliseconds