This module includes functions that control CoAP Secure (CoAP over DTLS) communication.
Macros |
|
#define | OT_DEFAULT_COAP_SECURE_PORT 5684 |
Default CoAP Secure port, as specified in RFC 7252.
|
Typedefs |
|
typedef void(* | otHandleCoapSecureClientConnect ) (bool aConnected, void *aContext) |
This function pointer is called when the DTLS connection state changes.
|
Functions |
|
otError | otCoapSecureStart ( otInstance *aInstance, uint16_t aPort) |
This function starts the CoAP Secure service.
|
|
void | otCoapSecureStop ( otInstance *aInstance) |
This function stops the CoAP Secure server.
|
|
void | otCoapSecureSetPsk ( otInstance *aInstance, const uint8_t *aPsk, uint16_t aPskLength, const uint8_t *aPskIdentity, uint16_t aPskIdLength) |
This method sets the Pre-Shared Key (PSK) and cipher suite DTLS_PSK_WITH_AES_128_CCM_8.
|
|
otError | otCoapSecureGetPeerCertificateBase64 ( otInstance *aInstance, unsigned char *aPeerCert, size_t *aCertLength, size_t aCertBufferSize) |
This method returns the peer x509 certificate base64 encoded.
|
|
void | otCoapSecureSetSslAuthMode ( otInstance *aInstance, bool aVerifyPeerCertificate) |
This method sets the authentication mode for the coap secure connection.
|
|
void | otCoapSecureSetCertificate ( otInstance *aInstance, const uint8_t *aX509Cert, uint32_t aX509Length, const uint8_t *aPrivateKey, uint32_t aPrivateKeyLength) |
This method sets the local device's X509 certificate with corresponding private key for DTLS session with DTLS_ECDHE_ECDSA_WITH_AES_128_CCM_8.
|
|
void | otCoapSecureSetCaCertificateChain ( otInstance *aInstance, const uint8_t *aX509CaCertificateChain, uint32_t aX509CaCertChainLength) |
This method sets the trusted top level CAs.
|
|
otError | otCoapSecureConnect ( otInstance *aInstance, const otSockAddr *aSockAddr, otHandleCoapSecureClientConnect aHandler, void *aContext) |
This method initializes DTLS session with a peer.
|
|
void | otCoapSecureDisconnect ( otInstance *aInstance) |
This method stops the DTLS connection.
|
|
bool | otCoapSecureIsConnected ( otInstance *aInstance) |
This method indicates whether or not the DTLS session is connected.
|
|
bool | otCoapSecureIsConnectionActive ( otInstance *aInstance) |
This method indicates whether or not the DTLS session is active.
|
|
otError | otCoapSecureSendRequestBlockWise ( otInstance *aInstance, otMessage *aMessage, otCoapResponseHandler aHandler, void *aContext, otCoapBlockwiseTransmitHook aTransmitHook, otCoapBlockwiseReceiveHook aReceiveHook) |
This method sends a CoAP request block-wise over secure DTLS connection.
|
|
otError | otCoapSecureSendRequest ( otInstance *aInstance, otMessage *aMessage, otCoapResponseHandler aHandler, void *aContext) |
This method sends a CoAP request over secure DTLS connection.
|
|
void | otCoapSecureAddResource ( otInstance *aInstance, otCoapResource *aResource) |
This function adds a resource to the CoAP Secure server.
|
|
void | otCoapSecureRemoveResource ( otInstance *aInstance, otCoapResource *aResource) |
This function removes a resource from the CoAP Secure server.
|
|
void | otCoapSecureAddBlockWiseResource ( otInstance *aInstance, otCoapBlockwiseResource *aResource) |
This function adds a block-wise resource to the CoAP Secure server.
|
|
void | otCoapSecureRemoveBlockWiseResource ( otInstance *aInstance, otCoapBlockwiseResource *aResource) |
This function removes a block-wise resource from the CoAP Secure server.
|
|
void | otCoapSecureSetDefaultHandler ( otInstance *aInstance, otCoapRequestHandler aHandler, void *aContext) |
This function sets the default handler for unhandled CoAP Secure requests.
|
|
void | otCoapSecureSetClientConnectedCallback ( otInstance *aInstance, otHandleCoapSecureClientConnect aHandler, void *aContext) |
This method sets the connected callback to indicate, when a Client connect to the CoAP Secure server.
|
|
otError | otCoapSecureSendResponseBlockWise ( otInstance *aInstance, otMessage *aMessage, const otMessageInfo *aMessageInfo, void *aContext, otCoapBlockwiseTransmitHook aTransmitHook) |
This function sends a CoAP response block-wise from the CoAP Secure server.
|
|
otError | otCoapSecureSendResponse ( otInstance *aInstance, otMessage *aMessage, const otMessageInfo *aMessageInfo) |
This function sends a CoAP response from the CoAP Secure server.
|
Detailed Description
This module includes functions that control CoAP Secure (CoAP over DTLS) communication.
The functions in this module are available when CoAP Secure API feature (
OPENTHREAD_CONFIG_COAP_SECURE_API_ENABLE
) is enabled.
Typedef Documentation
◆ otHandleCoapSecureClientConnect
typedef void(* otHandleCoapSecureClientConnect) (bool aConnected, void *aContext) |
This function pointer is called when the DTLS connection state changes.
- Parameters
-
[in] aConnected
true, if a connection was established, false otherwise. [in] aContext
A pointer to arbitrary context information.
Function Documentation
◆ otCoapSecureAddBlockWiseResource()
void otCoapSecureAddBlockWiseResource | ( | otInstance * |
aInstance,
|
otCoapBlockwiseResource * |
aResource
|
||
) |
This function adds a block-wise resource to the CoAP Secure server.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aResource
A pointer to the resource.
◆ otCoapSecureAddResource()
void otCoapSecureAddResource | ( | otInstance * |
aInstance,
|
otCoapResource * |
aResource
|
||
) |
This function adds a resource to the CoAP Secure server.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aResource
A pointer to the resource.
◆ otCoapSecureConnect()
otError otCoapSecureConnect | ( | otInstance * |
aInstance,
|
const otSockAddr * |
aSockAddr,
|
||
otHandleCoapSecureClientConnect |
aHandler,
|
||
void * |
aContext
|
||
) |
This method initializes DTLS session with a peer.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aSockAddr
A pointer to the remote socket address. [in] aHandler
A pointer to a function that will be called when the DTLS connection state changes. [in] aContext
A pointer to arbitrary context information.
- Return values
-
OT_ERROR_NONE
Successfully started DTLS connection.
◆ otCoapSecureDisconnect()
void otCoapSecureDisconnect | ( | otInstance * |
aInstance
|
) |
This method stops the DTLS connection.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.
◆ otCoapSecureGetPeerCertificateBase64()
otError otCoapSecureGetPeerCertificateBase64 | ( | otInstance * |
aInstance,
|
unsigned char * |
aPeerCert,
|
||
size_t * |
aCertLength,
|
||
size_t |
aCertBufferSize
|
||
) |
This method returns the peer x509 certificate base64 encoded.
- Note
-
This function requires the build-time features
MBEDTLS_BASE64_C
andMBEDTLS_SSL_KEEP_PEER_CERTIFICATE
to be enabled.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [out] aPeerCert
A pointer to the base64 encoded certificate buffer. [out] aCertLength
The length of the base64 encoded peer certificate. [in] aCertBufferSize
The buffer size of aPeerCert.
- Return values
-
OT_ERROR_INVALID_STATE
Not connected yet. OT_ERROR_NONE
Successfully get the peer certificate. OT_ERROR_NO_BUFS
Can't allocate memory for certificate.
◆ otCoapSecureIsConnected()
bool otCoapSecureIsConnected | ( | otInstance * |
aInstance
|
) |
This method indicates whether or not the DTLS session is connected.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.
- Return values
-
TRUE
The DTLS session is connected. FALSE
The DTLS session is not connected.
◆ otCoapSecureIsConnectionActive()
bool otCoapSecureIsConnectionActive | ( | otInstance * |
aInstance
|
) |
This method indicates whether or not the DTLS session is active.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.
- Return values
-
TRUE
If DTLS session is active. FALSE
If DTLS session is not active.
◆ otCoapSecureRemoveBlockWiseResource()
void otCoapSecureRemoveBlockWiseResource | ( | otInstance * |
aInstance,
|
otCoapBlockwiseResource * |
aResource
|
||
) |
This function removes a block-wise resource from the CoAP Secure server.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aResource
A pointer to the resource.
◆ otCoapSecureRemoveResource()
void otCoapSecureRemoveResource | ( | otInstance * |
aInstance,
|
otCoapResource * |
aResource
|
||
) |
This function removes a resource from the CoAP Secure server.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aResource
A pointer to the resource.
◆ otCoapSecureSendRequest()
otError otCoapSecureSendRequest | ( | otInstance * |
aInstance,
|
otMessage * |
aMessage,
|
||
otCoapResponseHandler |
aHandler,
|
||
void * |
aContext
|
||
) |
This method sends a CoAP request over secure DTLS connection.
If a response for a request is expected, respective function and context information should be provided. If no response is expected, these arguments should be NULL pointers. If Message Id was not set in the header (equal to 0), this function will assign unique Message Id to the message.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aMessage
A reference to the message to send. [in] aHandler
A function pointer that shall be called on response reception or time-out. [in] aContext
A pointer to arbitrary context information.
- Return values
-
OT_ERROR_NONE
Successfully sent CoAP message. OT_ERROR_NO_BUFS
Failed to allocate retransmission data. OT_ERROR_INVALID_STATE
DTLS connection was not initialized.
◆ otCoapSecureSendRequestBlockWise()
otError otCoapSecureSendRequestBlockWise | ( | otInstance * |
aInstance,
|
otMessage * |
aMessage,
|
||
otCoapResponseHandler |
aHandler,
|
||
void * |
aContext,
|
||
otCoapBlockwiseTransmitHook |
aTransmitHook,
|
||
otCoapBlockwiseReceiveHook |
aReceiveHook
|
||
) |
This method sends a CoAP request block-wise over secure DTLS connection.
This function is available when OPENTHREAD_CONFIG_COAP_BLOCKWISE_TRANSFER_ENABLE configuration is enabled.
If a response for a request is expected, respective function and context information should be provided. If no response is expected, these arguments should be NULL pointers. If Message Id was not set in the header (equal to 0), this function will assign unique Message Id to the message.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aMessage
A reference to the message to send. [in] aHandler
A function pointer that shall be called on response reception or time-out. [in] aContext
A pointer to arbitrary context information. [in] aTransmitHook
A function pointer that is called on Block1 response reception. [in] aReceiveHook
A function pointer that is called on Block2 response reception.
- Return values
-
OT_ERROR_NONE
Successfully sent CoAP message. OT_ERROR_NO_BUFS
Failed to allocate retransmission data. OT_ERROR_INVALID_STATE
DTLS connection was not initialized.
◆ otCoapSecureSendResponse()
otError otCoapSecureSendResponse | ( | otInstance * |
aInstance,
|
otMessage * |
aMessage,
|
||
const otMessageInfo * |
aMessageInfo
|
||
) |
This function sends a CoAP response from the CoAP Secure server.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aMessage
A pointer to the CoAP response to send. [in] aMessageInfo
A pointer to the message info associated with aMessage
.
- Return values
-
OT_ERROR_NONE
Successfully enqueued the CoAP response message. OT_ERROR_NO_BUFS
Insufficient buffers available to send the CoAP response.
◆ otCoapSecureSendResponseBlockWise()
otError otCoapSecureSendResponseBlockWise | ( | otInstance * |
aInstance,
|
otMessage * |
aMessage,
|
||
const otMessageInfo * |
aMessageInfo,
|
||
void * |
aContext,
|
||
otCoapBlockwiseTransmitHook |
aTransmitHook
|
||
) |
This function sends a CoAP response block-wise from the CoAP Secure server.
This function is available when OPENTHREAD_CONFIG_COAP_BLOCKWISE_TRANSFER_ENABLE configuration is enabled.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aMessage
A pointer to the CoAP response to send. [in] aMessageInfo
A pointer to the message info associated with aMessage
.[in] aContext
A pointer to arbitrary context information. May be NULL if not used. [in] aTransmitHook
A function pointer that is called on Block1 request reception.
- Return values
-
OT_ERROR_NONE
Successfully enqueued the CoAP response message. OT_ERROR_NO_BUFS
Insufficient buffers available to send the CoAP response.
◆ otCoapSecureSetCaCertificateChain()
void otCoapSecureSetCaCertificateChain | ( | otInstance * |
aInstance,
|
const uint8_t * |
aX509CaCertificateChain,
|
||
uint32_t |
aX509CaCertChainLength
|
||
) |
This method sets the trusted top level CAs.
It is needed for validating the certificate of the peer.
DTLS mode "ECDHE ECDSA with AES 128 CCM 8" for Application CoAPS.
- Note
-
This function requires
MBEDTLS_KEY_EXCHANGE_ECDHE_ECDSA_ENABLED=1
.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aX509CaCertificateChain
A pointer to the PEM formatted X509 CA chain. [in] aX509CaCertChainLength
The length of chain.
◆ otCoapSecureSetCertificate()
void otCoapSecureSetCertificate | ( | otInstance * |
aInstance,
|
const uint8_t * |
aX509Cert,
|
||
uint32_t |
aX509Length,
|
||
const uint8_t * |
aPrivateKey,
|
||
uint32_t |
aPrivateKeyLength
|
||
) |
This method sets the local device's X509 certificate with corresponding private key for DTLS session with DTLS_ECDHE_ECDSA_WITH_AES_128_CCM_8.
- Note
-
This function requires
MBEDTLS_KEY_EXCHANGE_ECDHE_ECDSA_ENABLED=1
.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aX509Cert
A pointer to the PEM formatted X509 certificate. [in] aX509Length
The length of certificate. [in] aPrivateKey
A pointer to the PEM formatted private key. [in] aPrivateKeyLength
The length of the private key.
◆ otCoapSecureSetClientConnectedCallback()
void otCoapSecureSetClientConnectedCallback | ( | otInstance * |
aInstance,
|
otHandleCoapSecureClientConnect |
aHandler,
|
||
void * |
aContext
|
||
) |
This method sets the connected callback to indicate, when a Client connect to the CoAP Secure server.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aHandler
A pointer to a function that will be called once DTLS connection is established. [in] aContext
A pointer to arbitrary context information. May be NULL if not used.
◆ otCoapSecureSetDefaultHandler()
void otCoapSecureSetDefaultHandler | ( | otInstance * |
aInstance,
|
otCoapRequestHandler |
aHandler,
|
||
void * |
aContext
|
||
) |
This function sets the default handler for unhandled CoAP Secure requests.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aHandler
A function pointer that shall be called when an unhandled request arrives. [in] aContext
A pointer to arbitrary context information. May be NULL if not used.
◆ otCoapSecureSetPsk()
void otCoapSecureSetPsk | ( | otInstance * |
aInstance,
|
const uint8_t * |
aPsk,
|
||
uint16_t |
aPskLength,
|
||
const uint8_t * |
aPskIdentity,
|
||
uint16_t |
aPskIdLength
|
||
) |
This method sets the Pre-Shared Key (PSK) and cipher suite DTLS_PSK_WITH_AES_128_CCM_8.
- Note
-
This function requires the build-time feature
MBEDTLS_KEY_EXCHANGE_PSK_ENABLED
to be enabled.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aPsk
A pointer to the PSK. [in] aPskLength
The PSK length. [in] aPskIdentity
The Identity Name for the PSK. [in] aPskIdLength
The PSK Identity Length.
◆ otCoapSecureSetSslAuthMode()
void otCoapSecureSetSslAuthMode | ( | otInstance * |
aInstance,
|
bool |
aVerifyPeerCertificate
|
||
) |
This method sets the authentication mode for the coap secure connection.
Disable or enable the verification of peer certificate. Must be called before start.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aVerifyPeerCertificate
true, to verify the peer certificate.
◆ otCoapSecureStart()
otError otCoapSecureStart | ( | otInstance * |
aInstance,
|
uint16_t |
aPort
|
||
) |
This function starts the CoAP Secure service.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aPort
The local UDP port to bind to.
- Return values
-
OT_ERROR_NONE
Successfully started the CoAP Secure server.
◆ otCoapSecureStop()
void otCoapSecureStop | ( | otInstance * |
aInstance
|
) |
This function stops the CoAP Secure server.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.