This structure represents a Server configuration.
#include <
include/openthread/netdata.h
>
Public Attributes | |
bool | mStable: 1 |
Whether this config is considered Stable Network Data. | |
uint8_t | mServerDataLength |
Length of server data. | |
uint8_t | mServerData [OT_SERVER_DATA_MAX_SIZE] |
Server data bytes. | |
uint16_t | mRloc16 |
The Server RLOC16. |
This structure represents a Server configuration.
The documentation for this struct was generated from the following file:
- include/openthread/
netdata.h