Plat-coprocessor-rpc
This module includes the platform abstraction for Co-processor RPC (CRPC) features.
Functions |
|
otError | otPlatCRPCProcess ( otInstance *aInstance, uint8_t aArgsLength, char *aArgs[], char *aOutput, size_t aOutputMaxLen) |
This function processes a Co-processor RPC command line.
|
Detailed Description
This module includes the platform abstraction for Co-processor RPC (CRPC) features.
Function Documentation
◆ otPlatCRPCProcess()
otError otPlatCRPCProcess | ( | otInstance * |
aInstance,
|
uint8_t |
aArgsLength,
|
||
char * |
aArgs[],
|
||
char * |
aOutput,
|
||
size_t |
aOutputMaxLen
|
||
) |
This function processes a Co-processor RPC command line.
- Parameters
-
[in] aInstance
The OpenThread instance for current request. [in] aArgsLength
The number of arguments in aArgs
.[in] aArgs
The arguments of command line. [out] aOutput
The execution result. [in] aOutputMaxLen
The output buffer size.
- Return values
-
OT_ERROR_INVALID_ARGS
The command is supported but invalid arguments provided. OT_ERROR_NONE
The command is successfully process. OT_ERROR_INVALID_COMMAND
The command is not valid or not supported.