otNetifMulticastAddress Struct Reference
This structure represents an IPv6 network interface multicast address.
#include <
include/openthread/ip6.h
>
Public Attributes | |
otIp6Address | mAddress |
The IPv6 multicast address. | |
const struct otNetifMulticastAddress * | mNext |
A pointer to the next network interface multicast address. |
This structure represents an IPv6 network interface multicast address.
The documentation for this struct was generated from the following file:
- include/openthread/
ip6.h