This module includes functions that allow a Host processor to execute remote procedure calls on a co-processor over spinel.
Functions | |
void | otCliAppendResult (otError aError) |
Append an error code to the output buffer. | |
otError | otCRPCHandleCommand (void *aContext, uint8_t aArgsLength, char *aArgs[], uint8_t aCommandsLength, const otCliCommand aCommands[]) |
Call the corresponding handler for a command. | |
void | otCliOutputBytes (const uint8_t *aBytes, uint8_t aLength) |
Output a byte array as hex to the output buffer. | |
void | otCliOutputCommands (const otCliCommand aCommands[], size_t aCommandsLength) |
Write all command names in aCommands to the output buffer. | |
int | otCliOutputFormatV (const char *aFormat, va_list aArguments) |
Write formatted output to the output buffer. | |
void | otCliOutputFormat (const char *aFmt,...) |
Write formatted string to the output buffer. | |
int | otCliOutputIp6Address (const otIp6Address *aAddress) |
Write an IPv6 address to the output buffer. | |
otError | otCRPCProcessCmd (uint8_t aArgsLength, char *aArgs[], char *aOutput, size_t aOutputMaxLen) |
Process a command line. | |
void | otCRPCProcessCmdLine (const char *aString, char *aOutput, size_t aOutputMaxLen) |
Process a command-line string. | |
otError | otCRPCProcessHelp (void *aContext, uint8_t aArgsLength, char *aArgs[]) |
Output all available CRPC built-in commands and user commands. | |
void | otCRPCSetUserCommands (const otCliCommand *aUserCommands, uint8_t aLength, void *aContext) |
Set a user command table. | |
char * | otCRPCGetStaticOutputBuffer (void) |
size_t | otCRPCGetStaticOutputBufferSize (void) |
Detailed Description
This module includes functions that allow a Host processor to execute remote procedure calls on a co-processor over spinel.
Function Documentation
◆ otCliAppendResult()
void otCliAppendResult | ( | otError | aError | ) |
Append an error code to the output buffer.
- Parameters
-
[in] aError
◆ otCliOutputBytes()
void otCliOutputBytes | ( | const uint8_t * | aBytes, |
uint8_t | aLength |
||
) |
Output a byte array as hex to the output buffer.
- Parameters
-
[in] aBytes
Bytes to output [in] aLength
Number of bytes
◆ otCliOutputCommands()
void otCliOutputCommands | ( | const otCliCommand | aCommands[], |
size_t | aCommandsLength |
||
) |
Write all command names in aCommands
to the output buffer.
- Parameters
-
[in] aCommands
an array of commands [in] aCommandsLength
length of aCommands
◆ otCliOutputFormat()
void otCliOutputFormat | ( | const char * | aFmt, |
... |
|||
) |
Write formatted string to the output buffer.
- Parameters
-
[in] aFmt
A pointer to the format string. [in] ...
A matching list of arguments.
◆ otCliOutputFormatV()
int otCliOutputFormatV | ( | const char * | aFormat, |
va_list | aArguments |
||
) |
Write formatted output to the output buffer.
- Parameters
-
[in] aFormat
A pointer to the format string. [in] aArguments
A variable list of arguments for format.
- Returns
- The number of bytes placed in the output buffer.
◆ otCliOutputIp6Address()
int otCliOutputIp6Address | ( | const otIp6Address * | aAddress | ) |
Write an IPv6 address to the output buffer.
- Parameters
-
[in] aAddress
A pointer to the IPv6 address.
- Returns
- The number of bytes placed in the output queue.
- Return values
-
-1
Driver is broken.
◆ otCRPCHandleCommand()
otError otCRPCHandleCommand | ( | void * | aContext, |
uint8_t | aArgsLength, |
||
char * | aArgs[], |
||
uint8_t | aCommandsLength, |
||
const otCliCommand | aCommands[] |
||
) |
Call the corresponding handler for a command.
This function will look through aCommands
to find a command that matches aArgs
[0]. If found, the handler function for the command will be called with the remaining args passed to it.
- Parameters
-
[in] aContext
a context [in] aArgsLength
number of args [in] aArgs
list of args [in] aCommandsLength
number of commands in aCommands
[in] aCommands
list of commands
- Return values
-
◆ otCRPCProcessCmd()
otError otCRPCProcessCmd | ( | uint8_t | aArgsLength, |
char * | aArgs[], |
||
char * | aOutput, |
||
size_t | aOutputMaxLen |
||
) |
Process a command line.
- Parameters
-
[in] aArgsLength
The number of elements in aArgs
.[in] aArgs
An array of arguments. [out] aOutput
The execution result. [in] aOutputMaxLen
The output buffer size.
- Return values
-
OT_ERROR_INVALID_ARGS
The command is supported but invalid arguments provided. OT_ERROR_NONE
The command is successfully process. OT_ERROR_NOT_IMPLEMENTED
The command is not supported.
◆ otCRPCProcessCmdLine()
void otCRPCProcessCmdLine | ( | const char * | aString, |
char * | aOutput, |
||
size_t | aOutputMaxLen |
||
) |
Process a command-line string.
- Parameters
-
[in] aString
A NULL-terminated input string. [out] aOutput
The execution result. [in] aOutputMaxLen
The output buffer size.
◆ otCRPCProcessHelp()
otError otCRPCProcessHelp | ( | void * | aContext, |
uint8_t | aArgsLength, |
||
char * | aArgs[] |
||
) |
Output all available CRPC built-in commands and user commands.
- Parameters
-
aContext
aArgsLength
aArgs
◆ otCRPCSetUserCommands()
void otCRPCSetUserCommands | ( | const otCliCommand * | aUserCommands, |
uint8_t | aLength, |
||
void * | aContext |
||
) |
Set a user command table.
- Parameters
-
[in] aUserCommands
A pointer to an array with user commands. [in] aLength
aUserCommands
length.[in] aContext
The
context passed to the handler.