This structure represents the Thread Leader Data.
#include <
include/openthread/thread.h
>
Public Attributes | |
uint32_t | mPartitionId |
Partition ID. | |
uint8_t | mWeighting |
Leader Weight. | |
uint8_t | mDataVersion |
Full Network Data Version. | |
uint8_t | mStableDataVersion |
Stable Network Data Version. | |
uint8_t | mLeaderRouterId |
Leader Router ID. |
This structure represents the Thread Leader Data.
The documentation for this struct was generated from the following file:
- include/openthread/
thread.h