otDnsTxtEntry Struct Reference

This structure represents a TXT record entry representing a key/value pair (RFC 6763 - section 6.3).

#include < include/openthread/dns.h >

Public Attributes

const char * mKey
The TXT record key string.
const uint8_t * mValue
The TXT record value or already encoded TXT-DATA (depending on mKey ).
uint16_t mValueLength
Number of bytes in mValue buffer.

This structure represents a TXT record entry representing a key/value pair (RFC 6763 - section 6.3).

The string buffers pointed to by mKey and mValue MUST persist and remain unchanged after an instance of such structure is passed to OpenThread (as part of otSrpClientService instance).

An array of otDnsTxtEntry entries are used in otSrpClientService to specify the full TXT record (a list of entries).

Member Data Documentation

◆ mKey

const char* otDnsTxtEntry::mKey

The TXT record key string.

If mKey is not NULL, then it MUST be a null-terminated C string. The entry is treated as key/value pair with mValue buffer providing the value.

  • The entry is encoded as follows:
    • A single string length byte followed by "key=value" format (without the quotation marks).
    • In this case, the overall encoded length must be 255 bytes or less.
  • If mValue is NULL, then key is treated as a boolean attribute and encoded as "key" (with no = ).
  • If mValue is not NULL but mValueLength is zero, then it is treated as empty value and encoded as "key=".

If mKey is NULL, then mValue buffer is treated as an already encoded TXT-DATA and is appended as is in the DNS message.


The documentation for this struct was generated from the following file:
  • include/openthread/ dns.h