otChildInfo Struct Reference

This structure holds diagnostic information for a Thread Child.

#include < include/openthread/thread_ftd.h >

Public Attributes

otExtAddress mExtAddress
IEEE 802.15.4 Extended Address.
uint32_t mTimeout
Timeout.
uint32_t mAge
Time last heard.
uint16_t mRloc16
RLOC16.
uint16_t mChildId
Child ID.
uint8_t mNetworkDataVersion
Network Data Version.
uint8_t mLinkQualityIn
Link Quality In.
int8_t mAverageRssi
Average RSSI.
int8_t mLastRssi
Last observed RSSI.
uint16_t mFrameErrorRate
Frame error rate (0xffff->100%). Requires error tracking feature.
uint16_t mMessageErrorRate
(IPv6) msg error rate (0xffff->100%). Requires error tracking feature.
uint16_t mQueuedMessageCnt
Number of queued messages for the child.
uint8_t mVersion
MLE version.
bool mRxOnWhenIdle : 1
rx-on-when-idle
bool mFullThreadDevice : 1
Full Thread Device.
bool mFullNetworkData : 1
Full Network Data.
bool mIsStateRestoring : 1
Is in restoring state.
bool mIsCslSynced : 1
Is child CSL synchronized.

This structure holds diagnostic information for a Thread Child.


The documentation for this struct was generated from the following file:
  • include/openthread/ thread_ftd.h