otTcpListener Struct Reference
This structure represents a TCP listener.
#include <
include/openthread/tcp.h
>
Public Attributes | |
union { | |
uint8_t mSize [OT_TCP_LISTENER_TCB_SIZE_BASE+OT_TCP_LISTENER_TCB_NUM_PTR *sizeof(void *)] | |
void * mAlign | |
} | mTcbListen |
struct otTcpListener * | mNext |
A pointer to the next TCP listener (internal use only) | |
void * | mContext |
A pointer to application-specific context. | |
otTcpAcceptReady | mAcceptReadyCallback |
"Accept ready" callback function | |
otTcpAcceptDone | mAcceptDoneCallback |
"Accept done" callback function |
This structure represents a TCP listener.
A TCP listener is used to listen for and accept incoming TCP connections.
The application should not inspect the fields of this structure directly; it should only interact with it via the TCP API functions whose signatures are provided in this file.
The documentation for this struct was generated from the following file:
- include/openthread/
tcp.h