otSrpClientHostInfo Struct Reference
This structure represents an SRP client host info.
#include <
include/openthread/srp_client.h
>
Public Attributes | |
const char * | mName |
Host name (label) string (NULL if not yet set). | |
const otIp6Address * | mAddresses |
Array of host IPv6 addresses (NULL if not set or auto address is enabled). | |
uint8_t | mNumAddresses |
Number of IPv6 addresses in mAddresses array. | |
bool | mAutoAddress |
Indicates whether auto address mode is enabled or not. | |
otSrpClientItemState | mState |
Host info state. |
This structure represents an SRP client host info.
The documentation for this struct was generated from the following file:
- include/openthread/
srp_client.h