Ping Sender
This file includes the OpenThread API for the ping sender module.
Classes | |
struct | otPingSenderReply |
This structure represents a ping reply. | |
struct | otPingSenderStatistics |
This structure represents statistics of a ping request. | |
struct | otPingSenderConfig |
This structure represents a ping request configuration. |
Typedefs | |
typedef struct otPingSenderReply | otPingSenderReply |
This structure represents a ping reply. | |
typedef struct otPingSenderStatistics | otPingSenderStatistics |
This structure represents statistics of a ping request. | |
typedef void(* | otPingSenderReplyCallback) (const otPingSenderReply *aReply, void *aContext) |
This function pointer type specifies the callback to notify receipt of a ping reply. | |
typedef void(* | otPingSenderStatisticsCallback) (const otPingSenderStatistics *aStatistics, void *aContext) |
This function pointer type specifies the callback to report the ping statistics. | |
typedef struct otPingSenderConfig | otPingSenderConfig |
This structure represents a ping request configuration. |
Functions | |
otError | otPingSenderPing (otInstance *aInstance, const otPingSenderConfig *aConfig) |
This function starts a ping. | |
void | otPingSenderStop (otInstance *aInstance) |
This function stops an ongoing ping. |
Detailed Description
This file includes the OpenThread API for the ping sender module.
Typedef Documentation
◆ otPingSenderReplyCallback
typedef void(* otPingSenderReplyCallback) (const otPingSenderReply *aReply, void *aContext) |
This function pointer type specifies the callback to notify receipt of a ping reply.
- Parameters
-
[in] aReply
A pointer to a otPingSenderReply
containing info about the received ping reply.[in] aContext
A pointer to application-specific context.
◆ otPingSenderStatisticsCallback
typedef void(* otPingSenderStatisticsCallback) (const otPingSenderStatistics *aStatistics, void *aContext) |
This function pointer type specifies the callback to report the ping statistics.
- Parameters
-
[in] aStatistics
A pointer to a otPingSenderStatistics
containing info about the received ping statistics.[in] aContext
A pointer to application-specific context.
Function Documentation
◆ otPingSenderPing()
otError otPingSenderPing | ( | otInstance * | aInstance, |
const otPingSenderConfig * | aConfig |
||
) |
This function starts a ping.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aConfig
The ping config to use.
- Return values
-
OT_ERROR_NONE
The ping started successfully. OT_ERROR_BUSY
Could not start since busy with a previous ongoing ping request. OT_ERROR_INVALID_ARGS
The aConfig
contains invalid parameters (e.g., ping interval is too long).
◆ otPingSenderStop()
void otPingSenderStop | ( | otInstance * | aInstance | ) |
This function stops an ongoing ping.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.