otJoinerDiscerner Struct Reference

This structure represents a Joiner Discerner.

#include <include/openthread/joiner.h>

Public Attributes

uint64_t mValue
 Discerner value (the lowest mLength bits specify the discerner).
 
uint8_t mLength
 Length (number of bits) - must be non-zero and at most OT_JOINER_MAX_DISCERNER_LENGTH.

This structure represents a Joiner Discerner.


The documentation for this struct was generated from the following file:
  • include/openthread/joiner.h