otExtAddress Struct Reference
This structure represents the IEEE 802.15.4 Extended Address.
#include <
include/openthread/platform/radio.h
>
Public Attributes | |
uint8_t | m8 [OT_EXT_ADDRESS_SIZE] |
IEEE 802.15.4 Extended Address bytes. |
This structure represents the IEEE 802.15.4 Extended Address.
The documentation for this struct was generated from the following file:
- include/openthread/platform/
radio.h