otNetworkName Struct Reference

This structure represents a Network Name.

#include < include/openthread/dataset.h >

Public Attributes

char m8 [ OT_NETWORK_NAME_MAX_SIZE +1]
Byte values. The + 1 is for null char.

This structure represents a Network Name.

The otNetworkName is a null terminated C string (i.e., m8 char array MUST end with null char \0 ).


The documentation for this struct was generated from the following file:
  • include/openthread/ dataset.h