otTcpEndpointInitializeArgs Struct Reference
This structure contains arguments to the otTcpEndpointInitialize() function.
#include <
include/openthread/tcp.h
>
Public Attributes | |
void * | mContext |
Pointer to application-specific context. | |
otTcpEstablished | mEstablishedCallback |
"Established" callback function | |
otTcpSendDone | mSendDoneCallback |
"Send done" callback function | |
otTcpForwardProgress | mForwardProgressCallback |
"Forward progress" callback function | |
otTcpReceiveAvailable | mReceiveAvailableCallback |
"Receive available" callback function | |
otTcpDisconnected | mDisconnectedCallback |
"Disconnected" callback function | |
void * | mReceiveBuffer |
Pointer to memory provided to the system for the TCP receive buffer. | |
size_t | mReceiveBufferSize |
Size of memory provided to the system for the TCP receive buffer. |
This structure contains arguments to the otTcpEndpointInitialize() function.
The documentation for this struct was generated from the following file:
- include/openthread/
tcp.h