otDnssdCounters Struct Reference
This structure contains the counters of DNS-SD server.
#include <
include/openthread/dnssd_server.h
>
Public Attributes | |
uint32_t | mSuccessResponse |
The number of successful responses. | |
uint32_t | mServerFailureResponse |
The number of server failure responses. | |
uint32_t | mFormatErrorResponse |
The number of format error responses. | |
uint32_t | mNameErrorResponse |
The number of name error responses. | |
uint32_t | mNotImplementedResponse |
The number of 'not implemented' responses. | |
uint32_t | mOtherResponse |
The number of other responses. | |
uint32_t | mResolvedBySrp |
The number of queries completely resolved by the local SRP server. |
This structure contains the counters of DNS-SD server.
The documentation for this struct was generated from the following file:
- include/openthread/
dnssd_server.h