otCommissioningDataset Struct Reference

This structure represents a Commissioning Dataset.

#include <include/openthread/commissioner.h>

Public Attributes

uint16_t mLocator
 Border Router RLOC16.
 
uint16_t mSessionId
 Commissioner Session Id.
 
otSteeringData mSteeringData
 Steering Data.
 
uint16_t mJoinerUdpPort
 Joiner UDP Port.
 
bool mIsLocatorSet: 1
 TRUE if Border Router RLOC16 is set, FALSE otherwise.
 
bool mIsSessionIdSet: 1
 TRUE if Commissioner Session Id is set, FALSE otherwise.
 
bool mIsSteeringDataSet: 1
 TRUE if Steering Data is set, FALSE otherwise.
 
bool mIsJoinerUdpPortSet: 1
 TRUE if Joiner UDP Port is set, FALSE otherwise.

This structure represents a Commissioning Dataset.


The documentation for this struct was generated from the following file:
  • include/openthread/commissioner.h