otEnergyScanResult Struct Reference

This structure represents an energy scan result.

#include <include/openthread/link.h>

Public Attributes

uint8_t mChannel
 IEEE 802.15.4 Channel.
 
int8_t mMaxRssi
 The max RSSI (dBm)

This structure represents an energy scan result.


The documentation for this struct was generated from the following file:
  • include/openthread/link.h