otSrpServerResponseCounters Struct Reference

This structure includes the statistics of SRP server responses.

#include <include/openthread/srp_server.h>

Public Attributes

uint32_t mSuccess
 The number of successful responses.
 
uint32_t mServerFailure
 The number of server failure responses.
 
uint32_t mFormatError
 The number of format error responses.
 
uint32_t mNameExists
 The number of 'name exists' responses.
 
uint32_t mRefused
 The number of refused responses.
 
uint32_t mOther
 The number of other responses.

This structure includes the statistics of SRP server responses.


The documentation for this struct was generated from the following file:
  • include/openthread/srp_server.h