This structure represents a received IEEE 802.15.4 Beacon.
#include <
include/openthread/link.h
>
Public Attributes | |
otExtAddress | mExtAddress |
IEEE 802.15.4 Extended Address. | |
otNetworkName | mNetworkName |
Thread Network Name. | |
otExtendedPanId | mExtendedPanId |
Thread Extended PAN ID. | |
otSteeringData | mSteeringData |
Steering Data. | |
uint16_t | mPanId |
IEEE 802.15.4 PAN ID. | |
uint16_t | mJoinerUdpPort |
Joiner UDP Port. | |
uint8_t | mChannel |
IEEE 802.15.4 Channel. | |
int8_t | mRssi |
RSSI (dBm) | |
uint8_t | mLqi |
LQI. | |
unsigned int | mVersion: 4 |
Version. | |
bool | mIsNative: 1 |
Native Commissioner flag. | |
bool | mDiscover: 1 |
Result from MLE Discovery. | |
bool | mIsJoinable: 1 |
Joining Permitted flag. |
This structure represents a received IEEE 802.15.4 Beacon.
The documentation for this struct was generated from the following file:
- include/openthread/
link.h