This structure represents the CoAP transmission parameters.
#include <
include/openthread/coap.h
>
Public Attributes | |
uint32_t | mAckTimeout |
Minimum spacing before first retransmission when ACK is not received, in milliseconds (RFC7252 default value is 2000ms). | |
uint8_t | mAckRandomFactorNumerator |
Numerator of ACK_RANDOM_FACTOR used to calculate maximum spacing before first retransmission when ACK is not received (RFC7252 default value of ACK_RANDOM_FACTOR is 1.5; must not be decreased below 1). | |
uint8_t | mAckRandomFactorDenominator |
Denominator of ACK_RANDOM_FACTOR used to calculate maximum spacing before first retransmission when ACK is not received (RFC7252 default value of ACK_RANDOM_FACTOR is 1.5; must not be decreased below 1). | |
uint8_t | mMaxRetransmit |
Maximum number of retransmissions for CoAP Confirmable messages (RFC7252 default value is 4). |
This structure represents the CoAP transmission parameters.
- Note
- mAckTimeout * ((2 ** (mMaxRetransmit + 1)) - 1) * (mAckRandomFactorNumerator / mAckRandomFactorDenominator) must not exceed what can be represented by a uint32_t (0xffffffff). This limitation allows OpenThread to avoid 64-bit arithmetic.
The documentation for this struct was generated from the following file:
- include/openthread/
coap.h