otPingSenderReply Struct Reference
This structure represents a ping reply.
#include <
include/openthread/ping_sender.h
>
Public Attributes | |
otIp6Address | mSenderAddress |
Sender IPv6 address (address from which ping reply was received). | |
uint16_t | mRoundTripTime |
Round trip time in msec. | |
uint16_t | mSize |
Data size (number of bytes) in reply (excluding IPv6 and ICMP6 headers). | |
uint16_t | mSequenceNumber |
Sequence number. | |
uint8_t | mHopLimit |
Hop limit. |
This structure represents a ping reply.
The documentation for this struct was generated from the following file:
- include/openthread/
ping_sender.h