otPlatTrelPeerInfo Struct Reference

This structure represents a TREL peer info discovered using DNS-SD browse on the service name "_trel._udp".

#include < include/openthread/platform/trel.h >

Public Attributes

bool mRemoved
This boolean flag indicates whether the entry is being removed or added.
const uint8_t * mTxtData
The TXT record data (encoded as specified by DNS-SD) from the SRV record of the discovered TREL peer service instance.
uint16_t mTxtLength
Number of bytes in mTxtData buffer.
otSockAddr mSockAddr
The TREL peer socket address (IPv6 address and port number).

This structure represents a TREL peer info discovered using DNS-SD browse on the service name "_trel._udp".

Member Data Documentation

◆ mRemoved

bool otPlatTrelPeerInfo::mRemoved

This boolean flag indicates whether the entry is being removed or added.

  • TRUE indicates that peer is removed.
  • FALSE indicates that it is a new entry or an update to an existing entry.

◆ mSockAddr

otSockAddr otPlatTrelPeerInfo::mSockAddr

The TREL peer socket address (IPv6 address and port number).

The port number is determined from the SRV record of the discovered TREL peer service instance. The IPv6 address is determined from the DNS-SD query for AAAA records on the hostname indicated in the SRV record of the discovered service instance. If multiple host IPv6 addressees are discovered, one with highest scope is used.


The documentation for this struct was generated from the following file:
  • include/openthread/platform/ trel.h