This structure represents a CoAP resource with block-wise transfer.
#include <
include/openthread/coap.h
>
Public Attributes | |
const char * | mUriPath |
The URI Path string. | |
otCoapRequestHandler | mHandler |
The callback for handling a received request. | |
otCoapBlockwiseReceiveHook | mReceiveHook |
The callback for handling incoming block-wise transfer. | |
otCoapBlockwiseTransmitHook | mTransmitHook |
The callback for handling outgoing block-wise transfer. | |
void * | mContext |
Application-specific context. | |
struct otCoapBlockwiseResource * | mNext |
The next CoAP resource in the list. |
This structure represents a CoAP resource with block-wise transfer.
Member Data Documentation
◆ mReceiveHook
otCoapBlockwiseReceiveHook otCoapBlockwiseResource::mReceiveHook |
The callback for handling incoming block-wise transfer.
This callback is available when OPENTHREAD_CONFIG_COAP_BLOCKWISE_TRANSFER_ENABLE configuration is enabled.
◆ mTransmitHook
otCoapBlockwiseTransmitHook otCoapBlockwiseResource::mTransmitHook |
The callback for handling outgoing block-wise transfer.
This callback is available when OPENTHREAD_CONFIG_COAP_BLOCKWISE_TRANSFER_ENABLE configuration is enabled.
The documentation for this struct was generated from the following file:
- include/openthread/
coap.h