otLinkedBuffer Struct Reference

A linked buffer structure for use with TCP.

#include < include/openthread/tcp.h >

Public Attributes

struct otLinkedBuffer * mNext
Pointer to the next linked buffer in the chain, or NULL if it is the end.
const uint8_t * mData
Pointer to data referenced by this linked buffer.
size_t mLength
Length of this linked buffer (number of bytes).

A linked buffer structure for use with TCP.

A single otLinkedBuffer structure references an array of bytes in memory, via mData and mLength. The mNext field is used to form a chain of otLinkedBuffer structures.


The documentation for this struct was generated from the following file:
  • include/openthread/ tcp.h