otSrpServerLeaseConfig Struct Reference

This structure includes SRP server LEASE and KEY-LEASE configurations.

#include <include/openthread/srp_server.h>

Public Attributes

uint32_t mMinLease
 The minimum LEASE interval in seconds.
 
uint32_t mMaxLease
 The maximum LEASE interval in seconds.
 
uint32_t mMinKeyLease
 The minimum KEY-LEASE interval in seconds.
 
uint32_t mMaxKeyLease
 The maximum KEY-LEASE interval in seconds.

This structure includes SRP server LEASE and KEY-LEASE configurations.


The documentation for this struct was generated from the following file:
  • include/openthread/srp_server.h