This structure represents a Network Diagnostic Route TLV value.
#include <
include/openthread/netdiag.h
>
Public Attributes | |
uint8_t | mIdSequence |
The sequence number associated with the set of Router ID assignments in mRouteData. | |
uint8_t | mRouteCount |
Number of elements in mRouteData. | |
otNetworkDiagRouteData | mRouteData [OT_NETWORK_MAX_ROUTER_ID+1] |
Link Quality and Routing Cost data. |
This structure represents a Network Diagnostic Route TLV value.
The documentation for this struct was generated from the following file:
- include/openthread/
netdiag.h