otDnsServiceInfo Struct Reference
This structure provides info for a DNS service instance.
#include <
include/openthread/dns_client.h
>
Public Attributes |
|
| uint32_t | mTtl |
|
Service record TTL (in seconds).
|
|
| uint16_t | mPort |
|
Service port number.
|
|
| uint16_t | mPriority |
|
Service priority.
|
|
| uint16_t | mWeight |
|
Service weight.
|
|
| char * | mHostNameBuffer |
|
Buffer to output the service host name (can be NULL if not needed).
|
|
| uint16_t | mHostNameBufferSize |
Size of
mHostNameBuffer
.
|
|
| otIp6Address | mHostAddress |
|
The host IPv6 address. Set to all zero if not available.
|
|
| uint32_t | mHostAddressTtl |
|
The host address TTL.
|
|
| uint8_t * | mTxtData |
|
Buffer to output TXT data (can be NULL if not needed).
|
|
| uint16_t | mTxtDataSize |
On input, size of
mTxtData
buffer. On output number bytes written.
|
|
| bool | mTxtDataTruncated |
Indicates if TXT data could not fit in
mTxtDataSize
and was truncated.
|
|
| uint32_t | mTxtDataTtl |
|
The TXT data TTL.
|
|
This structure provides info for a DNS service instance.
The documentation for this struct was generated from the following file:
-
include/openthread/
dns_client.h