otSecurityPolicy Struct Reference
This structure represent Security Policy.
#include <
include/openthread/dataset.h
>
Public Attributes | |
uint16_t | mRotationTime |
The value for thrKeyRotation in units of hours. | |
bool | mObtainNetworkKeyEnabled: 1 |
Obtaining the Network Key for out-of-band commissioning is enabled. | |
bool | mNativeCommissioningEnabled: 1 |
Native Commissioning using PSKc is allowed. | |
bool | mRoutersEnabled: 1 |
Thread 1.0/1.1.x Routers are enabled. | |
bool | mExternalCommissioningEnabled: 1 |
External Commissioner authentication is allowed. | |
bool | mCommercialCommissioningEnabled: 1 |
Commercial Commissioning is enabled. | |
bool | mAutonomousEnrollmentEnabled: 1 |
Autonomous Enrollment is enabled. | |
bool | mNetworkKeyProvisioningEnabled: 1 |
Network Key Provisioning is enabled. | |
bool | mTobleLinkEnabled: 1 |
ToBLE link is enabled. | |
bool | mNonCcmRoutersEnabled: 1 |
Non-CCM Routers enabled. | |
uint8_t | mVersionThresholdForRouting: 3 |
Version-threshold for Routing. |
This structure represent Security Policy.
The documentation for this struct was generated from the following file:
- include/openthread/
dataset.h