otPingSenderStatistics Struct Reference
This structure represents statistics of a ping request.
#include <
include/openthread/ping_sender.h
>
Public Attributes | |
uint16_t | mSentCount |
The number of ping requests already sent. | |
uint16_t | mReceivedCount |
The number of ping replies received. | |
uint32_t | mTotalRoundTripTime |
The total round trip time of ping requests. | |
uint16_t | mMinRoundTripTime |
The min round trip time among ping requests. | |
uint16_t | mMaxRoundTripTime |
The max round trip time among ping requests. | |
bool | mIsMulticast |
Whether this is a multicast ping request. |
This structure represents statistics of a ping request.
The documentation for this struct was generated from the following file:
- include/openthread/
ping_sender.h