This structure represents a Border Router configuration.
#include <
include/openthread/netdata.h
>
Public Attributes | |
otIp6Prefix | mPrefix |
The IPv6 prefix. | |
signed int | mPreference: 2 |
A 2-bit signed int preference (OT_ROUTE_PREFERENCE_* values). | |
bool | mPreferred: 1 |
Whether prefix is preferred. | |
bool | mSlaac: 1 |
Whether prefix can be used for address auto-configuration (SLAAC). | |
bool | mDhcp: 1 |
Whether border router is DHCPv6 Agent. | |
bool | mConfigure: 1 |
Whether DHCPv6 Agent supplying other config data. | |
bool | mDefaultRoute: 1 |
Whether border router is a default router for prefix. | |
bool | mOnMesh: 1 |
Whether this prefix is considered on-mesh. | |
bool | mStable: 1 |
Whether this configuration is considered Stable Network Data. | |
bool | mNdDns: 1 |
Whether this border router can supply DNS information via ND. | |
bool | mDp: 1 |
Whether prefix is a Thread Domain Prefix (added since Thread 1.2). | |
uint16_t | mRloc16 |
The border router's RLOC16 (value ignored on config add). |
This structure represents a Border Router configuration.
The documentation for this struct was generated from the following file:
- include/openthread/
netdata.h