Logging - Platform
This module includes the platform abstraction for the debug log service.
Macros | |
#define | OT_LOG_LEVEL_NONE 0 |
Log level None. | |
#define | OT_LOG_LEVEL_CRIT 1 |
Log level Critical. | |
#define | OT_LOG_LEVEL_WARN 2 |
Log level Warning. | |
#define | OT_LOG_LEVEL_NOTE 3 |
Log level Notice. | |
#define | OT_LOG_LEVEL_INFO 4 |
Log level Informational. | |
#define | OT_LOG_LEVEL_DEBG 5 |
Log level Debug. |
Typedefs | |
typedef int | otLogLevel |
This type represents the log level. | |
typedef enum otLogRegion | otLogRegion |
This enumeration represents log regions. |
Enumerations | |
enum | otLogRegion { OT_LOG_REGION_API = 1, OT_LOG_REGION_MLE = 2, OT_LOG_REGION_ARP = 3, OT_LOG_REGION_NET_DATA = 4, OT_LOG_REGION_ICMP = 5, OT_LOG_REGION_IP6 = 6, OT_LOG_REGION_TCP = 7, OT_LOG_REGION_MAC = 8, OT_LOG_REGION_MEM = 9, OT_LOG_REGION_NCP = 10, OT_LOG_REGION_MESH_COP = 11, OT_LOG_REGION_NET_DIAG = 12, OT_LOG_REGION_PLATFORM = 13, OT_LOG_REGION_COAP = 14, OT_LOG_REGION_CLI = 15, OT_LOG_REGION_CORE = 16, OT_LOG_REGION_UTIL = 17, OT_LOG_REGION_BBR = 18, OT_LOG_REGION_MLR = 19, OT_LOG_REGION_DUA = 20, OT_LOG_REGION_BR = 21, OT_LOG_REGION_SRP = 22, OT_LOG_REGION_DNS = 23 } |
This enumeration represents log regions. |
Functions | |
void | otPlatLog (otLogLevel aLogLevel, otLogRegion aLogRegion, const char *aFormat,...) |
This function outputs logs. | |
void | otPlatLogHandleLevelChanged (otLogLevel aLogLevel) |
This function handles OpenThread log level changes. |
Detailed Description
This module includes the platform abstraction for the debug log service.
Macro Definition Documentation
◆ OT_LOG_LEVEL_CRIT
#define OT_LOG_LEVEL_CRIT 1 |
Log level Critical.
- Note
- Log Levels are defines so that embedded implementations can eliminate code at compile time via #if/#else/#endif.
◆ OT_LOG_LEVEL_DEBG
#define OT_LOG_LEVEL_DEBG 5 |
Log level Debug.
- Note
- Log Levels are defines so that embedded implementations can eliminate code at compile time via #if/#else/#endif.
◆ OT_LOG_LEVEL_INFO
#define OT_LOG_LEVEL_INFO 4 |
Log level Informational.
- Note
- Log Levels are defines so that embedded implementations can eliminate code at compile time via #if/#else/#endif.
◆ OT_LOG_LEVEL_NONE
#define OT_LOG_LEVEL_NONE 0 |
Log level None.
- Note
- Log Levels are defines so that embedded implementations can eliminate code at compile time via #if/#else/#endif.
◆ OT_LOG_LEVEL_NOTE
#define OT_LOG_LEVEL_NOTE 3 |
Log level Notice.
- Note
- Log Levels are defines so that embedded implementations can eliminate code at compile time via #if/#else/#endif.
◆ OT_LOG_LEVEL_WARN
#define OT_LOG_LEVEL_WARN 2 |
Log level Warning.
- Note
- Log Levels are defines so that embedded implementations can eliminate code at compile time via #if/#else/#endif.
Typedef Documentation
◆ otLogRegion
typedef enum otLogRegion otLogRegion |
This enumeration represents log regions.
The support for log region is removed and instead each core module can define its own name to appended to the logs. However, the otLogRegion
enumeration is still defined as before to help with platforms which we may be using it in their otPlatLog()
implementation. The OT core will always emit all logs with OT_LOG_REGION_CORE
.
Enumeration Type Documentation
◆ otLogRegion
enum otLogRegion |
This enumeration represents log regions.
The support for log region is removed and instead each core module can define its own name to appended to the logs. However, the otLogRegion
enumeration is still defined as before to help with platforms which we may be using it in their otPlatLog()
implementation. The OT core will always emit all logs with OT_LOG_REGION_CORE
.
Function Documentation
◆ otPlatLog()
void otPlatLog | ( | otLogLevel | aLogLevel, |
otLogRegion | aLogRegion, |
||
const char * | aFormat, |
||
... |
|||
) |
This function outputs logs.
Note that the support for log region is removed. The OT core will always emit all logs with OT_LOG_REGION_CORE
as aLogRegion
.
- Parameters
-
[in] aLogLevel
The log level. [in] aLogRegion
The log region. [in] aFormat
A pointer to the format string. [in] ...
Arguments for the format specification.
◆ otPlatLogHandleLevelChanged()
void otPlatLogHandleLevelChanged | ( | otLogLevel | aLogLevel | ) |
This function handles OpenThread log level changes.
This platform function is called whenever the OpenThread log level changes. This platform function is optional since an empty weak implementation has been provided.
- Note
- Only applicable when
OPENTHREAD_CONFIG_LOG_LEVEL_DYNAMIC_ENABLE=1
.
- Parameters
-
[in] aLogLevel
The new OpenThread log level.