otTcpEndpoint Struct Reference
This structure represents a TCP endpoint.
#include <
include/openthread/tcp.h
>
Public Attributes |
|
union { | |
uint8_t
mSize
[
OT_TCP_ENDPOINT_TCB_SIZE_BASE
+OT_TCP_ENDPOINT_TCB_NUM_PTR
*sizeof(void *)] |
|
uint64_t mAlign | |
} | mTcb |
struct otTcpEndpoint * | mNext |
A pointer to the next TCP endpoint (internal use only)
|
|
void * | mContext |
A pointer to application-specific context.
|
|
otTcpEstablished | mEstablishedCallback |
"Established" callback function
|
|
otTcpSendDone | mSendDoneCallback |
"Send done" callback function
|
|
otTcpForwardProgress | mForwardProgressCallback |
"Forward progress" callback function
|
|
otTcpReceiveAvailable | mReceiveAvailableCallback |
"Receive available" callback function
|
|
otTcpDisconnected | mDisconnectedCallback |
"Disconnected" callback function
|
|
uint32_t | mTimers [4] |
otLinkedBuffer | mReceiveLinks [2] |
otSockAddr | mSockAddr |
uint8_t | mPendingCallbacks |
This structure represents a TCP endpoint.
An TCP endpoint acts an endpoint of TCP connection. It can be used to initiate TCP connections, and, once a TCP connection is established, send data to and receive data from the connection peer.
The application should not inspect the fields of this structure directly; it should only interact with it via the TCP API functions whose signatures are provided in this file.
The documentation for this struct was generated from the following file:
-
include/openthread/
tcp.h