otCacheEntryInfo Struct Reference
This structure represents an EID cache entry.
#include <
include/openthread/thread_ftd.h
>
Public Attributes | |
otIp6Address | mTarget |
Target EID. | |
otShortAddress | mRloc16 |
RLOC16. | |
otCacheEntryState | mState |
Entry state. | |
bool | mCanEvict: 1 |
Indicates whether the entry can be evicted. | |
bool | mValidLastTrans: 1 |
Indicates whether last transaction time and ML-EID are valid. | |
uint32_t | mLastTransTime |
Last transaction time (applicable in cached state). | |
otIp6Address | mMeshLocalEid |
Mesh Local EID (applicable if entry in cached state). | |
uint16_t | mTimeout |
Timeout in seconds (applicable if in snooped/query/retry-query states). | |
uint16_t | mRetryDelay |
Retry delay in seconds (applicable if in query-retry state). |
This structure represents an EID cache entry.
The documentation for this struct was generated from the following file:
- include/openthread/
thread_ftd.h