otBorderRoutingPrefixTableIterator Struct Reference
This structure represents an iterator to iterate through the Border Router's discovered prefix table.
#include <
include/openthread/border_routing.h
>
Public Attributes |
|
| const void * | mPtr1 |
| const void * | mPtr2 |
| uint32_t | mData32 |
This structure represents an iterator to iterate through the Border Router's discovered prefix table.
The fields in this type are opaque (intended for use by OpenThread core only) and therefore should not be accessed or used by caller.
Before using an iterator, it MUST be initialized using
otBorderRoutingPrefixTableInitIterator()
.
The documentation for this struct was generated from the following file:
-
include/openthread/
border_routing.h