Entropy
This module includes the platform abstraction for entropy generation.
Functions | |
otError | otPlatEntropyGet (uint8_t *aOutput, uint16_t aOutputLength) |
Fill buffer with entropy. |
Detailed Description
This module includes the platform abstraction for entropy generation.
Function Documentation
◆ otPlatEntropyGet()
otError otPlatEntropyGet | ( | uint8_t * | aOutput, |
uint16_t | aOutputLength |
||
) |
Fill buffer with entropy.
This function MUST be implemented using a true random number generator (TRNG).
- Parameters
-
[out] aOutput
A pointer to where the true random values are placed. Must not be NULL. [in] aOutputLength
Size of aBuffer
.
- Return values
-
OT_ERROR_NONE
Successfully filled aBuffer
with true random values.OT_ERROR_FAILED
Failed to fill aBuffer
with true random values.OT_ERROR_INVALID_ARGS
aBuffer
was set to NULL.