otPlatCryptoEcdsaSignature Struct Reference
This struct represents an ECDSA signature.
#include <
include/openthread/platform/crypto.h
>
Public Attributes |
|
| uint8_t | m8 [ OT_CRYPTO_ECDSA_SIGNATURE_SIZE ] |
This struct represents an ECDSA signature.
The signature is encoded as the concatenated binary representation of two MPIs
r
and
s
which are calculated during signing (RFC 6605 - section 4).
The documentation for this struct was generated from the following file:
-
include/openthread/platform/
crypto.h