otCryptoKey Struct Reference
This structure represents the Key Material required for Crypto operations.
#include <
include/openthread/platform/crypto.h
>
Public Attributes | |
const uint8_t * | mKey |
Pointer to the buffer containing key. NULL indicates to use mKeyRef . | |
uint16_t | mKeyLength |
The key length in bytes (applicable when mKey is not NULL). | |
uint32_t | mKeyRef |
The PSA key ref (requires mKey to be NULL). |
This structure represents the Key Material required for Crypto operations.
The documentation for this struct was generated from the following file:
- include/openthread/platform/
crypto.h