otLinkMetricsValues Struct Reference

This structure represents the result (value) for a Link Metrics query.

#include < include/openthread/link_metrics.h >

Public Attributes

otLinkMetrics mMetrics
Specifies which metrics values are present/included.
uint32_t mPduCountValue
The value of Pdu Count.
uint8_t mLqiValue
The value LQI.
uint8_t mLinkMarginValue
The value of Link Margin.
int8_t mRssiValue
The value of Rssi.

This structure represents the result (value) for a Link Metrics query.


The documentation for this struct was generated from the following file:
  • include/openthread/ link_metrics.h