This module includes functions for child supervision feature.
Functions | |
uint16_t | otChildSupervisionGetInterval (otInstance *aInstance) |
Get the child supervision interval (in seconds). | |
void | otChildSupervisionSetInterval (otInstance *aInstance, uint16_t aInterval) |
Set the child supervision interval (in seconds). | |
uint16_t | otChildSupervisionGetCheckTimeout (otInstance *aInstance) |
Get the supervision check timeout interval (in seconds). | |
void | otChildSupervisionSetCheckTimeout (otInstance *aInstance, uint16_t aTimeout) |
Set the supervision check timeout interval (in seconds). |
Detailed Description
This module includes functions for child supervision feature.
The functions in this module are available when child supervision feature (OPENTHREAD_CONFIG_CHILD_SUPERVISION_ENABLE
) is enabled.
Function Documentation
◆ otChildSupervisionGetCheckTimeout()
uint16_t otChildSupervisionGetCheckTimeout | ( | otInstance * | aInstance | ) |
Get the supervision check timeout interval (in seconds).
If the device is a sleepy child and it does not hear from its parent within the specified check timeout, it initiates the re-attach process (MLE Child Update Request/Response exchange with its parent).
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.
- Returns
- The supervision check timeout. Zero indicates that supervision check on the child is disabled.
◆ otChildSupervisionGetInterval()
uint16_t otChildSupervisionGetInterval | ( | otInstance * | aInstance | ) |
Get the child supervision interval (in seconds).
Child supervision feature provides a mechanism for parent to ensure that a message is sent to each sleepy child within the supervision interval. If there is no transmission to the child within the supervision interval, OpenThread enqueues and sends a supervision message (a data message with empty payload) to the child.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.
- Returns
- The child supervision interval. Zero indicates that child supervision is disabled.
◆ otChildSupervisionSetCheckTimeout()
void otChildSupervisionSetCheckTimeout | ( | otInstance * | aInstance, |
uint16_t | aTimeout |
||
) |
Set the supervision check timeout interval (in seconds).
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aTimeout
The check timeout (in seconds). Zero to disable supervision check on the child.
◆ otChildSupervisionSetInterval()
void otChildSupervisionSetInterval | ( | otInstance * | aInstance, |
uint16_t | aInterval |
||
) |
Set the child supervision interval (in seconds).
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aInterval
The supervision interval (in seconds). Zero to disable supervision on parent.