otNeighborInfo Struct Reference

This structure holds diagnostic information for a neighboring Thread node.

#include <include/openthread/thread.h>

Public Attributes

otExtAddress mExtAddress
 IEEE 802.15.4 Extended Address.
 
uint32_t mAge
 Time last heard.
 
uint16_t mRloc16
 RLOC16.
 
uint32_t mLinkFrameCounter
 Link Frame Counter.
 
uint32_t mMleFrameCounter
 MLE Frame Counter.
 
uint8_t mLinkQualityIn
 Link Quality In.
 
int8_t mAverageRssi
 Average RSSI.
 
int8_t mLastRssi
 Last observed RSSI.
 
uint16_t mFrameErrorRate
 Frame error rate (0xffff->100%). Requires error tracking feature.
 
uint16_t mMessageErrorRate
 (IPv6) msg error rate (0xffff->100%). Requires error tracking feature.
 
bool mRxOnWhenIdle: 1
 rx-on-when-idle
 
bool mFullThreadDevice: 1
 Full Thread Device.
 
bool mFullNetworkData: 1
 Full Network Data.
 
bool mIsChild: 1
 Is the neighbor a child.

This structure holds diagnostic information for a neighboring Thread node.


The documentation for this struct was generated from the following file:
  • include/openthread/thread.h