otNetifAddress Struct Reference
This structure represents an IPv6 network interface unicast address.
#include <
include/openthread/ip6.h
>
Public Attributes | |
otIp6Address | mAddress |
The IPv6 unicast address. | |
uint8_t | mPrefixLength |
The Prefix length (in bits). | |
uint8_t | mAddressOrigin |
The IPv6 address origin. | |
bool | mPreferred: 1 |
TRUE if the address is preferred, FALSE otherwise. | |
bool | mValid: 1 |
TRUE if the address is valid, FALSE otherwise. | |
bool | mScopeOverrideValid: 1 |
TRUE if the mScopeOverride value is valid, FALSE otherwise. | |
unsigned int | mScopeOverride: 4 |
The IPv6 scope of this address. | |
bool | mRloc: 1 |
TRUE if the address is an RLOC, FALSE otherwise. | |
struct otNetifAddress * | mNext |
A pointer to the next network interface address. |
This structure represents an IPv6 network interface unicast address.
The documentation for this struct was generated from the following file:
- include/openthread/
ip6.h