otOperationalDataset Struct Reference
This structure represents an Active or Pending Operational Dataset.
#include <
include/openthread/dataset.h
>
Public Attributes |
|
| uint64_t | mActiveTimestamp |
|
Active Timestamp.
|
|
| uint64_t | mPendingTimestamp |
|
Pending Timestamp.
|
|
| otNetworkKey | mNetworkKey |
|
Network Key.
|
|
| otNetworkName | mNetworkName |
|
Network Name.
|
|
| otExtendedPanId | mExtendedPanId |
|
Extended PAN ID.
|
|
| otMeshLocalPrefix | mMeshLocalPrefix |
|
Mesh Local Prefix.
|
|
| uint32_t | mDelay |
|
Delay Timer.
|
|
| otPanId | mPanId |
|
PAN ID.
|
|
| uint16_t | mChannel |
|
Channel.
|
|
| otPskc | mPskc |
|
PSKc.
|
|
| otSecurityPolicy | mSecurityPolicy |
|
Security Policy.
|
|
| otChannelMask | mChannelMask |
|
Channel Mask.
|
|
| otOperationalDatasetComponents | mComponents |
|
Specifies which components are set in the Dataset.
|
|
This structure represents an Active or Pending Operational Dataset.
Components in Dataset are optional.
mComponets
structure specifies which components are present in the Dataset.
The documentation for this struct was generated from the following file:
-
include/openthread/
dataset.h