SPI Slave
This module includes the platform abstraction for SPI slave communication.
Typedefs | |
typedef bool(* | otPlatSpiSlaveTransactionCompleteCallback) (void *aContext, uint8_t *aOutputBuf, uint16_t aOutputBufLen, uint8_t *aInputBuf, uint16_t aInputBufLen, uint16_t aTransactionLength) |
Indicates that a SPI transaction has completed with the given length. | |
typedef void(* | otPlatSpiSlaveTransactionProcessCallback) (void *aContext) |
Invoked after a transaction complete callback is called and returns TRUE to do any further processing required. |
Functions | |
otError | otPlatSpiSlaveEnable (otPlatSpiSlaveTransactionCompleteCallback aCompleteCallback, otPlatSpiSlaveTransactionProcessCallback aProcessCallback, void *aContext) |
Initialize the SPI slave interface. | |
void | otPlatSpiSlaveDisable (void) |
Shutdown and disable the SPI slave interface. | |
otError | otPlatSpiSlavePrepareTransaction (uint8_t *aOutputBuf, uint16_t aOutputBufLen, uint8_t *aInputBuf, uint16_t aInputBufLen, bool aRequestTransactionFlag) |
Prepare data for the next SPI transaction. |
Detailed Description
This module includes the platform abstraction for SPI slave communication.
Typedef Documentation
◆ otPlatSpiSlaveTransactionCompleteCallback
typedef bool(* otPlatSpiSlaveTransactionCompleteCallback) (void *aContext, uint8_t *aOutputBuf, uint16_t aOutputBufLen, uint8_t *aInputBuf, uint16_t aInputBufLen, uint16_t aTransactionLength) |
Indicates that a SPI transaction has completed with the given length.
The data written to the slave has been written to the pointer indicated by the aInputBuf
argument to the previous call to otPlatSpiSlavePrepareTransaction()
.
Once this function is called, otPlatSpiSlavePrepareTransaction()
is invalid and must be called again for the next transaction to be valid.
Note that this function is always called at the end of a transaction, even if otPlatSpiSlavePrepareTransaction()
has not yet been called. In such cases, aOutputBufLen
and aInputBufLen
will be zero.
This callback can be called from ISR context. The return value from this function indicates if any further processing is required. If TRUE
is returned the platform spi-slave driver implementation must invoke the transaction process callback (aProcessCallback
set in otPlatSpiSlaveEnable()
) which unlike this callback must be called from the same OS context that any other OpenThread API/callback is called.
- Parameters
-
[in] aContext
Context pointer passed into otPlatSpiSlaveEnable()
.[in] aOutputBuf
Value of aOutputBuf
from last call tootPlatSpiSlavePrepareTransaction()
.[in] aOutputBufLen
Value of aOutputBufLen
from last call tootPlatSpiSlavePrepareTransaction()
.[in] aInputBuf
Value of aInputBuf from last call to otPlatSpiSlavePrepareTransaction()
.[in] aInputBufLen
Value of aInputBufLen from last call to otPlatSpiSlavePrepareTransaction()
[in] aTransactionLength
Length of the completed transaction, in bytes.
- Returns
- TRUE if after this call returns the platform should invoke the process callback
aProcessCallback
, FALSE if there is nothing to process and no need to invoke the process callback.
◆ otPlatSpiSlaveTransactionProcessCallback
typedef void(* otPlatSpiSlaveTransactionProcessCallback) (void *aContext) |
Invoked after a transaction complete callback is called and returns TRUE
to do any further processing required.
Unlike otPlatSpiSlaveTransactionCompleteCallback
which can be called from any OS context (e.g., ISR), this callback MUST be called from the same OS context as any other OpenThread API/callback.
- Parameters
-
[in] aContext
Context pointer passed into otPlatSpiSlaveEnable()
.
Function Documentation
◆ otPlatSpiSlaveEnable()
otError otPlatSpiSlaveEnable | ( | otPlatSpiSlaveTransactionCompleteCallback | aCompleteCallback, |
otPlatSpiSlaveTransactionProcessCallback | aProcessCallback, |
||
void * | aContext |
||
) |
Initialize the SPI slave interface.
Note that SPI slave is not fully ready until a transaction is prepared using otPlatSPISlavePrepareTransaction()
.
If otPlatSPISlavePrepareTransaction() is not called before the master begins a transaction, the resulting SPI transaction will send all
0xFF` bytes and discard all received bytes.
- Parameters
-
[in] aCompleteCallback
Pointer to transaction complete callback. [in] aProcessCallback
Pointer to process callback. [in] aContext
Context pointer to be passed to callbacks.
- Return values
-
OT_ERROR_NONE
Successfully enabled the SPI Slave interface. OT_ERROR_ALREADY
SPI Slave interface is already enabled. OT_ERROR_FAILED
Failed to enable the SPI Slave interface.
◆ otPlatSpiSlavePrepareTransaction()
otError otPlatSpiSlavePrepareTransaction | ( | uint8_t * | aOutputBuf, |
uint16_t | aOutputBufLen, |
||
uint8_t * | aInputBuf, |
||
uint16_t | aInputBufLen, |
||
bool | aRequestTransactionFlag |
||
) |
Prepare data for the next SPI transaction.
Data pointers MUST remain valid until the transaction complete callback is called by the SPI slave driver, or until after the next call to otPlatSpiSlavePrepareTransaction()
.
This function may be called more than once before the SPI master initiates the transaction. Each successful call to this function will cause the previous values from earlier calls to be discarded.
Not calling this function after a completed transaction is the same as if this function was previously called with both buffer lengths set to zero and aRequestTransactionFlag
set to false
.
Once aOutputBufLen
bytes of aOutputBuf
has been clocked out, the MISO pin shall be set high until the master finishes the SPI transaction. This is the functional equivalent of padding the end of aOutputBuf
with 0xFF
bytes out to the length of the transaction.
Once aInputBufLen
bytes of aInputBuf have been clocked in from MOSI, all subsequent values from the MOSI pin are ignored until the SPI master finishes the transaction.
Note that even if aInputBufLen
or aOutputBufLen
(or both) are exhausted before the SPI master finishes a transaction, the ongoing size of the transaction must still be kept track of to be passed to the transaction complete callback. For example, if aInputBufLen
is equal to 10 and aOutputBufLen
equal to 20 and the SPI master clocks out 30 bytes, the value 30 is passed to the transaction complete callback.
If a NULL
pointer is passed in as aOutputBuf
or aInputBuf
it means that that buffer pointer should not change from its previous/current value. In this case, the corresponding length argument should be ignored. For example, otPlatSpiSlavePrepareTransaction(NULL, 0, aInputBuf, aInputLen, false)
changes the input buffer pointer and its length but keeps the output buffer pointer same as before.
Any call to this function while a transaction is in progress will cause all of the arguments to be ignored and the return value to be OT_ERROR_BUSY
.
- Parameters
-
[in] aOutputBuf
Data to be written to MISO pin [in] aOutputBufLen
Size of the output buffer, in bytes [in] aInputBuf
Data to be read from MOSI pin [in] aInputBufLen
Size of the input buffer, in bytes [in] aRequestTransactionFlag
Set to true if host interrupt should be set
- Return values
-
OT_ERROR_NONE
Transaction was successfully prepared. OT_ERROR_BUSY
A transaction is currently in progress. OT_ERROR_INVALID_STATE
otPlatSpiSlaveEnable() hasn't been called.