otSrpClientService Struct Reference

This structure represents an SRP client service.

#include < include/openthread/srp_client.h >

Public Attributes

const char * mName
The service name labels (e.g., "_chip._udp", not the full domain name).
const char * mInstanceName
The service instance name label (not the full name).
const char *const * mSubTypeLabels
Array of service sub-type labels (must end with NULL or can be NULL ).
const otDnsTxtEntry * mTxtEntries
Array of TXT entries (number of entries is given by mNumTxtEntries ).
uint16_t mPort
The service port number.
uint16_t mPriority
The service priority.
uint16_t mWeight
The service weight.
uint8_t mNumTxtEntries
Number of entries in the mTxtEntries array.
otSrpClientItemState mState
uint32_t mData
Internal data (used by OT core).
struct otSrpClientService * mNext
Pointer to next entry in a linked-list (managed by OT core).

This structure represents an SRP client service.

The values in this structure, including the string buffers for the names and the TXT record entries, MUST persist and stay constant after an instance of this structure is passed to OpenThread from otSrpClientAddService() or otSrpClientRemoveService() .

Member Data Documentation

◆ mState

otSrpClientItemState otSrpClientService::mState
Note
The following fields are used/managed by OT core only. Their values do not matter and are ignored when an instance of otSrpClientService is passed in otSrpClientAddService() or otSrpClientRemoveService() . The user should not modify these fields.Service state (managed by OT core).

The documentation for this struct was generated from the following file:
  • include/openthread/ srp_client.h