This structure holds diagnostic information for a Thread Router.
#include <
include/openthread/thread.h
>
Public Attributes | |
otExtAddress | mExtAddress |
IEEE 802.15.4 Extended Address. | |
uint16_t | mRloc16 |
RLOC16. | |
uint8_t | mRouterId |
Router ID. | |
uint8_t | mNextHop |
Next hop to router. | |
uint8_t | mPathCost |
Path cost to router. | |
uint8_t | mLinkQualityIn |
Link Quality In. | |
uint8_t | mLinkQualityOut |
Link Quality Out. | |
uint8_t | mAge |
Time last heard. | |
bool | mAllocated: 1 |
Router ID allocated or not. | |
bool | mLinkEstablished: 1 |
Link established with Router ID or not. |
This structure holds diagnostic information for a Thread Router.
The documentation for this struct was generated from the following file:
- include/openthread/
thread.h