otBackboneRouterConfig Struct Reference
This structure represents Backbone Router configuration.
#include <
include/openthread/backbone_router.h
>
Public Attributes | |
uint16_t | mServer16 |
Only used when get Primary Backbone Router information in the Thread Network. | |
uint16_t | mReregistrationDelay |
Reregistration Delay (in seconds) | |
uint32_t | mMlrTimeout |
Multicast Listener Registration Timeout (in seconds) | |
uint8_t | mSequenceNumber |
Sequence Number. |
This structure represents Backbone Router configuration.
The documentation for this struct was generated from the following file:
- include/openthread/
backbone_router.h